AXIS#.VL.LMJR

Description

This parameter is used in the internal calculation of the current loop acceleration feed forward gain value.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

NA

Range

0 to 100.0

Default Value

0

Data Type

Float
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
AXIS1.VL.LMJR

5011h

0bh

Unsigned32

-

1000:1

Read/Write

No

AXIS2.VL.LMJR

5111h

0bh

Unsigned32

-

1000:1

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.VL.LMJR

6033

1791

Unsigned32

Read/Write

-

AXIS2.VL.LMJR

71569

1179

Unsigned32

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.VL.LMJR

6033

Float

Read/Write

-